Part Number: LP-MSPM0G3507
I am attempting to use the back UART connection on a Mac for the first time. Port enumerates as expected. When connect from the Terminal of CCS, or other 3rd party terminal to the enumerated UART port, I see no traffic on TX when probing with an oscilloscope. Also bridged RX/TX, to see the response back to the host - nothing is observable. MacOS is at 12.6.8
UART works under Windows when switching to a VM on the same computer.
Is there any known issue with the UART port on MacOS?