Part Number: MSPM0G1507
Hi, It's not clear to me as to why the reset cause values are different between the MSPM0 G-Series Technical Reference Manual (section 2.6.1.32 RSTCAUSE Register) and the
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G1507
Hi, It's not clear to me as to why the reset cause values are different between the MSPM0 G-Series Technical Reference Manual (section 2.6.1.32 RSTCAUSE Register) and the
Hi Bryan,
I opened the files and compared the enum values to the TRM. I found them to match

This is on SDK 1.10 and the TRM that is currently online on TI.com
Regards,
Luke
Hi Luke,
Which source file are you showing in your reply? It's something other than dl_sysctl_mspm0g1x0x_g3x0x.h. Maybe the issue is just with the hover over feature, which shows values different than expected for this.

Hi Bryan,
I'm getting different results when I hover over

From my original screenshot, I did CTRL+Left Click on the right side of the "=" to get to the actual value. I was using CCS 12.4 when checking this. I switched over to CCS Theia and can confirm what you are seeing with the value of 6. When I go to the file it should pull the right side of the "=" from, it is properly set. See mspm0_sdk_1_10_00_05/source/ti/devices/msp.peripherals/m0p/sysctl/hw_sysctl_mspm0g1x0x_g3x0x.h
I will check that this is a visual bug and get to investigating why the value is appearing incorrect.
Regards,
Luke