Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: UNIFLASH
I'm trying to build the QSPI SBL example for the AM263x LaunchPad from source unsuccessfully.
I think something is wrong with the resulting binary, because I load it to flash with uniflash, then set the boot mode pins to UART boot mode (like below), then reset the board, and I see XMODEM output as if the board dip switches were set to UART boot mode. I realize this boot pin configuration sets the RBL fallback mode to UART, so I think that means that QSPI RBL is failing.
Both the sbl_qspi.debug.tiimage and sbl_qspi.release.tiimage prebuilt SBLs packaged at tools/boot/sbl_prebuilt/am263x-lp work, so I think my individual board isn't causing this problem.
I'm using MCU+SDK 08_06_00_34, and I imported the SBL QSPI example into CCS from this MCU+SDK directory: examples/drivers/boot/sbl_qspi/am263x-lp/r5fss0-0_nortos I built the SBL without changing anything after importing.
I've also tried adding the `loop_forever()` function to the top of main() in the example QSPI SBL source like suggested here, however CPU execution isn't in that loop when I connect the debugger, which supports my thought that QSPI RBL is failing. https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1119575/faq-mcu-plus-sdk-am243x-how-to-debug-sbl_qspi-for-am263-and-am273-or-sbl_ospi-for-am243-or-an-application-which-is-booted-via-ospi-qspi-boot
This is what my uniflash.cfg file looks like:
# First point to sbl_uart_uniflash binary, which function's as a server to flash one or more files --flash-writer=/home/amacgregor/ti/mcu_plus_sdk_am263x_08_06_00_34/tools/boot/sbl_prebuilt/am263x-lp/sbl_uart_uniflash.release.tiimage # When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0 --file=/opt/ti/ccs_2023_workspace_v12/sbl_qspi_am263x-lp_r5fss0-0_nortos_ti-arm-clang/Debug/sbl_qspi_am263x-lp_r5fss0-0_nortos_ti-arm-clang.tiimage --operation=flash --flash-offset=0x0

What steps can I take to debug this further and end up with a compiling QSPI SBL source code that I can customize?
Thank you,
-Andy