Part Number: AM2634
When I run the example on the launchpad, I get a maximum stable bandwidth of 10-15 Mbps. If it is more, we have missing or out of order frames. Also, when I run iperf with the 100 Mbit flag - the terminal actually shows 1 Mbit.
Command in the console of the PC:
iperf.exe -c 192.168.100.100 -r -u -t 1 -b 100m
Is it possible to get a bandwidth of about 100 Mbps?
What do we need to do to get more bandwidth?