Part Number: TMS570LC4357
Hello everyone,
My project consists of two distinct parts: a "BootLoader" and an "Application". I want the application start from a special address such as 0x00004000, but the application can't upload properly.
I’m a bit confused about it.
I face several challenges:
1. I cannot change the bootloader and application startup address
I have changed the addresses in my code but cannot upload (I have a bus error generated by CPU). I read that I had to change an address in HL_sys_intvecs.asm but I did not understand.
2. How do I properly configure the interrupt vectors for the Boot Loader and the Application?
I would be grateful if someone could give me advice. If you have already done a similar task, I would love to hear your experience.
Thanks in advance for your help!