Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: MSPM0L1306
OS: Win 10
Browser: Chrome
OOBE URL: https://dev.ti.com/gallery/view/7473522/LP_MSPM0L1306_OOBE/ver/1.0.0/
Problem: With the Browser loaded with the Out of Box Example (OOBE), the example fails to connect with the development board.
Hello:
These are the steps I used when attempting to make the browser-based OOBE GUI example connect with the dev board.
- Connected the board to the USB port of my computer.
- Navigated to the OOBE URL.
- Clicked on the link icon, located on the lower-left corner of the browser window, to create a connection, but the response was "Error Loading Program for MSPM0L1306 Device Failed: Missing Extension."
Steps I took in trying to diagnose and fix the problem.
- Ran the Device Manager, then inspected the properties for the XDS110 Class Application/User UART device, and then adjusted the serial communication settings to match the requirements. See attached image.
- From the Main Menu of the browser, clicked on File, then selected Load Program, but received the following error message: Load Program Failed: Loading Program for MSPM0L1306 Device Failed: Missing Extension." See attached image.
- From the Main Menu of the browser, clicked on Options, then selected Serial Port Settings..., but no resulting action occurred.
- Ran a serial communications console (Putty), and then I was able to connect with the dev board. When I pressed S2, messages were sent to the console which were received by the console. See attached image.
What can I do to create the connection so this OOBE will work?