Part Number: MSP432E401Y
Hi,
I need help converting this example to something that will work with the MSP432E4 SDK and CCS 12.4.0.
#define MULADDC_INIT \
asm(
#define MULADDC_CORE \
"ldr r0, [%0], #4 \n\t" \
"ldr r1, [%1] \n\t" \
"umaal r1, %2, %3, r0 \n\t" \
"str r1, [%1], #4 \n\t"
#define MULADDC_STOP \
: "=r" (s), "=r" (d), "=r" (c) \
: "r" (b), "0" (s), "1" (d), "2" (c) \
: "r0", "r1", "memory" \
);
Thanks,
-Mike