Dear Champs,
Is there any way to load HSM firmware on HSFS device(SR1.1) before fusing customer keys?
Thanks and Best Regards,
SI.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
Is there any way to load HSM firmware on HSFS device(SR1.1) before fusing customer keys?
Thanks and Best Regards,
SI.
Hi SI,
HSM Run Time firmware load is supported in both HS-FS and HS-SE devices. The difference between the same are mentioned here -
https://dev.ti.com/tirex/explore/node?node=A__AV7JOFQElxyKdMz93HO.9w__AM26X-ACADEMY__t0CaxbG__LATEST
For User Modified Custom HSM Firmware, they need HS-SE devices.
Best Regards,
Aakash
Hi Aakash,
Thanks for the clarification.
BTW, what is HSM Run Time firmware?
When I checked MCU+ SDK UG, HSM Server is one of HSM runtime firmware we provide through MCU+ SDK, right?
Is it possible to download User modified customer HSM FIrmware after turning to HS-SE device?
My customer want to release their product with user modified HSM FIrmware on HS-FS device, and then, run user modified HSM FIrmware after signing HS-SE device. Is this scenario possible?
Thanks and Best Regards,
SI.
Hi Sung-IL ,
HSM Server is one of HSM runtime firmware we provide through MCU+ SDK, right?
Actually TIFS-MCU Firmware is TI's HSM Firmware delivered to the customers. HSM Server is a communication model between HSM Firmware and Application (which will act as a HSM Client).
Is it possible to download User modified customer HSM FIrmware after turning to HS-SE device?
Customer needs to request for NDA as mentioned in the Academy. This will allow them to use TIFS-MCU package.
My customer want to release their product with user modified HSM FIrmware on HS-FS device, and then, run user modified HSM FIrmware after signing HS-SE device. Is this scenario possible?
No, TI owns the HSM Run-Time Firmware in case of HS-FS devices to provide easy development of applications etc. However, to ensure customer freedom of use in case of HSM Firmware, the HS-SE devices are introduced with root of trust with the customers.
Anyways, HS-FS devices are deemed non-secure and fit for development. However, HS-SE devices are considered secure and fit for production.
Best Regards,
Aakash