Part Number: TMS570LC4357-EP
Hello Support Team,
We are planning to use TMS570LC4347-EP in our projects because of its lockstep feature. However DO-178C standards limit us, so that we would like to ask you some questions;
1- How does the lockstep feature work in TMS570LC4347-EP?
2- Is it possible to use split mode with TMS570LC4347-EP?
3- Can the second core work independently?
4- If 3rd question is not, how does the second core use memory? Same or different?
5- If both cores uses same memory, how are the input registers of both core designed?
6- In the technical reference, there was a figure (in page 499 figure 13-1.Block Diagram) and it seems there are two independent input registers for both core but this is a discrete case of lockstep phenomenon, can you explain this figure as well?
Thank you in advance for your answers,
Halil