Part Number: TM4C1290NCPDT
Hi Team:
My customer trying to use TM4C1290NCPDT with passive crystal oscillator in their system.
As pre check with customer, after the reset signal is pulled high, it takes 15ms for the TM4C1290NCPDT to start up normally after the external passive crystal oscillator is turned on. Please help me to confirm the following questions, thank you
1. For the 12ms low level of the crystal oscillator after the reset signal is pulled high, can it be judged that the crystal oscillator is not driven to start oscillation at this time?
2. After the reset signal is pulled high and the chip starts to run from the main function, how long does it take? Is it about 12ms?
3. customer tested other TI`s DSP chip on their side, and the passive crystal oscillator starts running as soon as it is powered on. There is no need to wait too much. Please briefly explain the difference between DSP and MCU for passive crystal oscillator configuration?
4. if we think that 1290N recommends the use of active crystal oscillators, please also provide reasons why passive crystal oscillators are not suitable.
tks for your confirmation.