Part Number: AM2431
Other Parts Discussed in Thread: LP-AM243
I want to load FreeRTOS and 1Gbps Ethernet/IP adapter on AM2431 without external RAM
AM2431 has 2MB of internal RAM.
Is this RAM enough?
Thank you for reading it. Please reply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to load FreeRTOS and 1Gbps Ethernet/IP adapter on AM2431 without external RAM
I have few question before I can answer that:
1. Are you implementing your own ethernetIP stck at 1Gbps.
2. What is the memory foot print of it.
Could you please let me know what your memory requirement for Ethernet IP 1g is? Anyways you could always use GPMC interface to connect an extra RAM. Apart from that you have upto 2GB DDR memory available in ALV package . Please check below data sheet for more details.