Part Number: MSPM0G1507
Hi Champs!
I received question from customer:
With the MSPM0 I use the FCC to monitor the PLL frequency.
In order to be able to use the FCC, I have so far accessed the external 32 KHz.
In the new manual (SLAU846 - JUNE 2023), under "2.3.5 Frequency Clock Counter (FCC)" I read that the internal 32 KHz of the SYSOSC can also be used as a source. This was not documented in a previous Early Sample manual.
In the “Figure 2-8. MSPM0Gxx Top Level Clocking Tree”, as in the older manual, only external CLKs are specified.
Can the FCC now also be used with the internal LFOSC?
If so, can this source also be used with the watchdog and is the LFOSC (int. 32 KHz) independent of the PLL?
B R Dirk