Part Number: MSPM0L1306
Dear Apps experts,
I one of my customers has an issue using MSPM0L with XDS110 debugger in IAR.
To give you an overview of the issue:
The customer has the:
mspm0_sdk_1_10_00_05
and used the
guide to run MSPM0 using IAR.
He just installed the required drivers and the TIXDS
I managed to help him setting the environment paths
But now he has the following problem using the XDS emulator:

Updating the XDS works and can run the following commands:
xdsdfu.exe -m
-xdsdfu.exe -f firmware_3.0.0.26.bin -r
I also pointed the customer to the following manual:
Is there anything I am missing and that could cause this issue ?
Regards,
Alex