Part Number: MSP432E401Y
Hi TI!
I need to use USB + 2xCAN but there are pinout conflict.
PIN95 CAN1_RX or USB0ID
PIN96 CAN1_TX or USBVBUS
1-) Can I use the USB without the USB0ID and USBVBUS signals and leave them as CAN?
2-) To connect to the CAN network do I need a driver like MAXIM's MAX3051 or similar?
Thank you very much! Best reagards!