Part Number: MCU-PLUS-SDK-AM243X
Hello IT-Support,
i think the Build-in Self-test functionality is insufficient documented.
Additional it is a Build-in Self-test when a Core test the other Cores and not itself?
There is no documentation how the Build in Self-Tests work exactly. How the PBIST procedure work exactly?
It can only use the fixed defines in sdlr_soc_pbist.h (like: SDL_PBIST2_ALGO_BITMAP_0) to make a config setup (with the PBIST_TestHandle_t structure) like in the examples.
There is no explanation (in API, code) which fixed defines (PBIST2) are for which instance (found out with spruim2g.pdf - Table 5-838).
There is no explanation how to setup this structure correct.
What is important to consider, when i want to use the BIST?
Can I change the fixed defines (like SDL_PBIST2_ALGO_BITMAP_0) ?