This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: ADC for MSP432E401Y

Part Number: MSP432E401Y

Hi TI!!!

I need to measure the voltage of 8 DC sources with maximum value of 24V. For this I will use a voltage divider with two resistors of 100k and 15k, so I take a sample of approx. 3.13V when the voltage to be measured is 24V (maximum), please see the schematic.

My question is if I can take the voltage sample directly from the resistive divider to the MSP432E401 pin or should I put an operational amplifier (between the resistive divider and the MSP432 ) with gain = 1 to acquire the voltage sample from a low impedance source?

Another question:
For the 8 input pins of the ADC I plan to use PD0,...PD7. There is no problem with this 8 pins to read the analog voltage samples, right?