Part Number: LP-AM243
Other Parts Discussed in Thread: AM6442, UNIFLASH
Hi all TI expert,
I have a problem on LP-243 bring up,
I followed the document step, try to bring up the develop board, link like below,
my environment:
Platform: Windows
SDK: mcu_plus_sdk_am243x_09_00_00_30
In the dfu-util step, I got problem, my dfu-util version is dfu-util 0.8

then in
Steps to install windows generic USB drivers.
In the zadig, even I list all device in the Options, I can't found the AM64x DFU this device,
I also found another topic discuss about the AM6442 dfu issue.
In this case, into SDK folder, /tools/boot/usb_dfu_uniflash.py, use python to execute this file,
use the command like below,
python usb_dfu_uniflash.py --cfg=sbl_prebuilt\am64x-evm\default_dfu_ospi.cfg
Because we used different develop board, so made some change, the correct command like below,
python usb_dfu_uniflash.py --cfg=sbl_prebuilt\am243x-lp\default_dfu_ospi.cfg

File not found, then I found in the default_dfu_ospi.cfg file, 31 lines, indicate to a not exist file,