This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3107: Mass erase procedure using Segger J-Link w/ Ozone debugger.. BSL Invocation..

Part Number: MSPM0G3107

My customer has the following questions..

Currently I have a concern regarding restoring microcontroller after lockup.

For me, the lockup happens often, after each exception leading to hard fault. After that default reflasing with SWD does not work and I keep getting (Error -614 @ 0x0)

I know about mass erase procedure from the presentation: /cfs-file/__key/communityserver-discussions-components-files/908/Unlock-MSPM0.pptx

I know how to invoke BSL as described in https://www.ti.com/lit/pdf/slau319

 

My questions are:

  1. How can the mass erase procedure above be invoked using Segger J-Link and Ozone debugger (or any other standard JTAG probe/environment outside CCS)?
  2. Alternatively, for development purposes: can BSL be invoked without using PA18?

Thx, Merril

  • Hi Merril,

    For Q1:

    At the moment, support for DSSM commands is implemented using CCS or the DSSM Unlock GUI tool with XDS110 (Mass erase need completed by DSSM).

    For Q2;

    It can invoke without PA18, and have two workarounds:

    1. Using other hardware pin, it can be modified in NONMAIN.

    2.disable hardware invoke pin via NONMAIN, then it can run into bsl with a software invoke, which means that you need do some modficiations in application code.

    B.R.

    Sal