Other Parts Discussed in Thread: SYSCONFIG
Hi, I'm currently using Sysconfig GUI 1.17 with MOTOR CONTROL SDK (09.00.00), when I tried to choose the device as either AM263x or AM243x and click start, it would pop up the following error:
soc.getClockSourceOptions is not a function
TypeError: soc.getClockSourceOptions is not a function
at loaderFunc (C:\Users\a0505397\git\testing\motor_control_sdk\mcu_plus_sdk\source\drivers\.meta\uart\v2\uart_v2.syscfg.js:94:31)
at func (webpack:///src/pinmux/services/resources/metaContentLoaders/resourceLoader.ts:238:45)
at Object.internalBoundary (webpack:///src/pinmux/services/niceExceptions.ts:43:10)
at t.ResourceLoader.loadResource (webpack:///src/pinmux/services/resources/metaContentLoaders/resourceLoader.ts:238:22)
at t.ResourceLoader.getResource (webpack:///src/pinmux/services/resources/metaContentLoaders/resourceLoader.ts:338:15)
at Object.getScript (webpack:///src/pinmux/services/resources/runtime.ts:91:25)
at getModule (C:\Users\a0505397\git\testing\motor_control_sdk\mcu_plus_sdk\source\drivers\.meta\uart\uart.syscfg.js:9:19)
at loaderFunc (C:\Users\a0505397\git\testing\motor_control_sdk\mcu_plus_sdk\source\drivers\.meta\uart\uart.syscfg.js:12:11)
at func (webpack:///src/pinmux/services/resources/metaContentLoaders/resourceLoader.ts:238:45)
at Object.t.internalBoundary (webpack:///src/pinmux/services/niceExceptions.ts:43:10)
This is the configuration I used to produce this error message:

I'm not sure if this is an isolated problem on my end, but if it is, please suggest any methods to address this.
Best,
Sen Wang