Part Number: AM2732
Other Parts Discussed in Thread: TIDA-020047, AWR2243
Hi,
I used the mmwave demo to integrate the cascading of 2xAWR2243, I used following configuration and it fails when configuring the slave radar.
char* radarCmdString[MAX_RADAR_CMD] =
{
"sensorStop\n\r",
"flushCfg\n\r",
"dfeDataOutputMode 1\n\r",
"channelCfg 15 7 0\n\r",
"adcCfg 2 1\n\r",
"adcbufCfg -1 0 1 1 1\n\r",
"lowPower 0 1\n\r",
"dataPathClkCfg 1 1\n\r",
"profileCfg 0 77 267 7 57.14 0 0 70 1 256 5209 0 0 30\n\r",
"dataPathConfig 0 1 0 2 64 64 64 0\n\r",
"hsiClockConfig 9 0\n\r",
"hsiLaneConfig 15 1 0 2 0 4 0 5 0 3 0 0\n\r",
"dataFormatConfig 1 1\n\r",
"chirpCfg 0 0 0 0 0 0 0 1\n\r",
"chirpCfg 1 1 0 0 0 0 0 4\n\r",
"chirpCfg 2 2 0 0 0 0 0 2\n\r",
"frameCfg 0 2 16 0 256 100 2 0\n\r",
"guiMonitor -1 1 1 0 0 0 1\n\r",
"cfarCfg -1 0 2 8 4 3 0 15 1\n\r",
"cfarCfg -1 1 0 4 2 3 1 15 1\n\r",
"multiObjBeamForming -1 1 0.5\n\r",
"calibDcRangeSig -1 0 -5 8 256\n\r",
"clutterRemoval -1 0\n\r",
"compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0\n\r",
"measureRangeBiasAndRxChanPhase 0 1.5 0.2\n\r",
"aoaFovCfg -1 -90 90 -90 90\n\r",
"cfarFovCfg -1 0 0 8.92\n\r",
"cfarFovCfg -1 1 -1 1.00\n\r",
"extendedMaxVelocity -1 0\n\r",
"calibData 0 0 0\n\r",
"sensorStart\n\r"
};
Could you please give me a correct configuration which works with the 2xAWR2243 ?
Thanks.