Other Parts Discussed in Thread: BQ25180
Hi,
I am working on a project in which I required a battery charging module.
Below are the specifications of battery (GRP333736-3.8V-385mAh) which I am using:
Typical Capacity : 385mAh
Minimum Capacity :370mAh
Nominal Voltage :3.8V
Max.Charge Current :385mA(1C)
Max.Charge Voltage : 4.35V
Nominal Continuous Discharge Current : 192.5mA(0.5C)
Max. Continuous Discharge Current : 385mA(1C)
Max. Continuous Discharge Rate : 1C
Cut-off Voltage : 3.0V
According to Impedance tracking algorithm, it is required to divide the charge by 10 of battery capacity. So, I'd like to know if there is any module whose lowest charging limit is 10mA, as the normal capacity of the batteries used in my project is 385mAh.
The datasheet of the above mentioned module is attached herewith.