Part Number: TMS570LC4357
Hello,
During the use of MPU, it was found that there are two descriptions in the manual that cannot be found in the register description. Please help to confirm:
1,
In the description of the NMPU chapter, it is mentioned that when the NMPU lock step comparison error occurs, the DIAGERR in the MPUERRSTAT register can be set to 1. However, after querying the description of the MPUERRSTAT register, it was found that there is no description of the DIAGERR bit in the register field.


2. The MPUREGAM0-7, MPUYREGTA0-7, and MPUREGMT0-7 described in the MPUREGNUM register are not mentioned in the register field and NMPU context.

Regards,
Gary