Part Number: MSPM0G3507
Hi,
I am new to CCS topics, therefore I decided to ask here for support.
I need to debug multiple (.out) files using a single Debug Configuration inside Code Composer Studio (v12.4.0).
Previously on my projects I used IAR Debugger where I had the possibility to flash/debug a main .elf file with up to 3 additional .elf files inside debug options.
Here in CCS, when I have to select the debug image (.out file), I see that I can only select one single file, I don't have an option to add secondary images.
Can someone help me with some hints?
Thank you in advance!