This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-RTOS-MCU: Download of TI-RTOS installers halts after downloading a few megabytes

Part Number: TI-RTOS-MCU


curl -O https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/tirtos/2_21_01_08/exports/tirtos_cc13xx_cc26xx_setuplinux_2_21_01_08.bin
% Total % Received % Xferd Average Speed Time Time Time Current
Dload Upload Total Spent Left Speed
12 143M 12 18.0M 0 0 7966k 0 0:00:18 0:00:02 0:00:16 7968k
curl: (18) transfer closed with 131769779 bytes remaining to read

Link is from this page.

https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/tirtos/index.html

Same error when downloading via browser. Same error for the Windows and MacOS installers.

Thank you for investigating.

  • Hi Alexei,

    I am not experiencing the same issue currently with Windows 10 on Chrome or Linux Ubuntu 22.04 with Firefox, so perhaps it was a temporary issue with the TI website.  Otherwise check your internet connection stability and try another data retrieval command such as wget.  Also state what OSs you are attempting if you continue to experience issue.

    Regards,
    Ryan

  • Works now. But, something definitely changed, because now the server replies with a 302 redirect. This redirect was not happening at the time of making the original post.

    curl -L -O software-dl.ti.com/.../tirtos_cc13xx_cc26xx_setuplinux_2_21_01_08.bin
    % Total % Received % Xferd Average Speed Time Time Time Current
    Dload Upload Total Spent Left Speed
    100 420 100 420 0 0 1749 0 --:--:-- --:--:-- --:--:-- 1757
    0 0 0 0 0 0 0 0 --:--:-- --:--:-- --:--:-- 0
    100 143M 100 143M 0 0 5031k 0 0:00:29 0:00:29 --:--:-- 3515k