Part Number: AM2434
Hello there,
I am looking into the specifications of AM 2434. In this context, I would like to know the contact operation time at high temperature operation.
The UM contains the following statement. For example, if the temperature is below Tj 105°C, does this mean that the device can operate continuously for 10000 hours?

If not, what are the conditions for 10 years of continuous operation?
Best regards,
Ryuto