Part Number: MSPM0G3507
Hi,
My customer is looking for a SPI that will run in Stop or Standby. Looks from the DS that our SPIs are in the PD1 domain on the block diagram and colored yellow (PD1). However is section 17.2.1 Clock Control of the TRM it implies the SPI instance can be in PD0.
Can you clarify if the TRM was being generic and the DS says PD1 or is there ability to run the SPI in the lower power domain?
Best Regards,
Blake