Hi Sir
I want to control the UART0 of Main from M4F MCU domain.
The address of UART0 are traslated by RAT but the UART0 still can't be control.
How can I do it?



BR
ShengYi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
I want to control the UART0 of Main from M4F MCU domain.
The address of UART0 are traslated by RAT but the UART0 still can't be control.
How can I do it?



BR
ShengYi
Hello,
The MCU domain is isolated from the rest of the SOC. According to the Table 12-440 and Figure 12-236 in the TRM, the main UART cannot be accessed from MCU domain. Section 1.4 shows the purpose of isolating the MCU domain from faults in the rest of the SOC.
Thank you,
Anita
hi Sir
Thank you for your answer. Could the MCAN control by MCU domian.
if the MCAN can control by MCU domain,How can I do it?

BR
Sheng Yi
Hello Sheng Yi,
The MCU domain cannot control MCAN from main domain also. This is not a feasible option.
Thank you,
Anita