Part Number: MSPM0G3507
Hello,
I have a lot of parts where non main memory was reflashed more than one time
At some point there is no access possible to the part
I try the procedure described in 0726.Factory_reset_v2
instead of seeing the reset, it seems it can't connect to the part, then it stays stuck on this window

CS_DAP_0: GEL Output: Initiating Device Factory Reset
CS_DAP_0: GEL Output: Attempting CS_DAP connection
CS_DAP_0: GEL Output: Attempting SEC_AP connection
CS_DAP_0: GEL Output: Command Sent
CS_DAP_0: GEL Output: Start hardware Reset using NRST
CS_DAP_0: GEL Output: Initiating BOOTRST Board Reset
CS_DAP_0: GEL Output: Reset line asserted
CS_DAP_0: GEL Output: Reset line de-asserted
CS_DAP_0: GEL Output: Board Reset Complete
CS_DAP_0: GEL Output: Reset done
CS_DAP_0: GEL Output: SEC_AP Disconnect
CS_DAP_0: GEL Output: SEC_AP Reconnect
is there anything else I can do except changing the microcontroler?
Thanks