Other Parts Discussed in Thread: SYSCONFIG
I'm trying to integrate Marvell PHY drivers into the AM263x TI MCU+ SDK CPSW ethernet drivers. The Marvell driver expects a XMDIO interface for register reads/writes that uses Clause-45 frames. In the sysconfig tool, I have configured the MDIO Clause-45 PHY mask to the PHY addresses I'm using. When the Mdio_open function tries to open the MDIO, it checks to see if this mask is set and returns ENET_ENOTSUPPORTED. However the AM263x TRM states that the CPSW supports Clause-45 frames: "13.2.1.1.1 CPSW0 Features - Management Data Input/Output (MDIO) module for PHY Management with Clause 45 support".