Hi Nilabh,
The problem about the device with fiemware v9.0.0.3 can’t change the IP configuration mode by Rockwell EtherNet/IP Address Commissioning Tool is described here.
- When we use the tool to send the request to change the IP configuration mode to “Static”, the
tool responds the device don’t support CIP and the mode change fail.
We wonder if it’s also a firmware issue, and if it could be fixed.
The WireShark data is as below.
Thank you for the support.
Bo-Cheng