Part Number: MCU-PLUS-SDK-AM243X
Hello,
so we updated to SDK 08.06 but suddenly some of our interrupts did not work anymore.
Previously we needed to manipulate the boardcfg for rm. We use 4 mcu-pins as interrupts and therefore we needed to change one assigned ressource to M4F to R5F_0_0 in the sciclient_defaultBoardcfg_rm.c. That works. I updated the SDK and saw that now this setting is default in the sciclient_defaultBoardcfg_rm.c and thought I do not need to do anything then and can use the default boardcfg from now on. unfortunately It did not work once. No interrupt came up.
Since we created the interrupts manually based on the example, since SysCfg did not generate the interrupts before, I checked what SysCfg would do with the same settings now and it used a CSLR_R5FSS0_CORE0_INTR_MAIN_GPIOMUX_INTROUTER0_OUTP_X instead of an CSLR_R5FSS0_CORE0_INTR_MCU_MCU_GPIOMUX_INTROUTER0_OUTP_X, that we used before. I am not sure but that sounds wrong?
Also somehow for a tisci_msg_rm_irq_release_req.src_id for MCU there is an offset by 30 now used as a base. Before it was just the raw pin-number.
So we did not get it to work and just used the old boardcfg again (without that 30+ offset for mcu src-index) and everything worked.
We then checked what is different and tried to generate our own board-cfg new and here we saw a change in the boardcfg-generation. previously the python blob-gen had a dev-grp option set to 0. now it is DEVGRP_MAIN. when we changed it back to 0 it works with the new SDK-generated boardcfg.
It's this place in the makefile at tools/sysfw/boardcfg/makefile:
$(PYTHON) $(BLOB_GEN) --sw-rev 1 --devgrp $(DEVGRP_MAIN) --bcfg $(BCFG) --bcfg-rm $(BCFG_RM) --bcfg-pm $(BCFG_PM) --bcfg-sec $(BCFG_SEC) --output-file $(BCFG_BLOB_FILE)
and how it looked before (changing --devGrp back to 0 works!)
$(PYTHON) $(BLOB_GEN) --sw-rev 1 --devgrp 0 --bcfg $(BCFG) --bcfg-rm $(BCFG_RM) --bcfg-pm $(BCFG_PM) --bcfg-sec $(BCFG_SEC) --output-file $(BCFG_BLOB_FILE)
Unfortunately also without any code-changes at our side and without that 30+ index for MCU.
Are there still some small mistakes in the boardcfg-creation and in the interrupt-routing? Or did we understand something wrong?
Also the RESPART-Tool does not really work for us. it somehow destroys our SysCfg-installations or throws a lot of different errors.
Best regards
Felix