Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I am hoping to configure the MSPM0 device as a Controller for 2 peripherals.
This would be a 4 wire connection between controller and peripheral with separate CS lines as shown below.
Is there anything within the MSPM0 software which would allow me to have multiple chip selects? Essentially is there some internal connection within the MSPM0 to allow for an easier CS method for two lines or will I need to configure the CS line as a digital output and manually write to the CS line when writing to SPI.
Any guidance on how these 5 signals should be connected to the MCU would be much appreciated.

Best Regards,
Elizabeth