Hi,
Need to remove memory dump commands as part of security hardening from code based used [u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3 .following memory dump commands should be disabled.
can you confirm if these commands are part of uboot code based delivered from TI-SDK-ti-processor-sdk-linux-am437x-hs-evm-06.03.00.106
In u boot commands , following memory dump commands should be disabled.
|
md : Memory Display command. mm : Memory modify command - auto incrementing address. nm : Memory modify command - constant address. mw : Memory write. cp : Memory copy. mwc : Memory write cyclic. mdc : Memory display cyclic. mtest : Simple ram read/write test. loopw : Infinite write loop on address range. |
FYI-
The source code for most of the commands in the u-boot can be found at u-boot/common/. These files usually start with cmd_*