This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Max Speed



Hello TI-Engineers,

For availability reasons I plan to run two TMS570 MCUs in dual active mode. Therefore i want to connect then by  a UART Line (UART Signals are transported by LDVS Transceivers). In the MCU Manual I found that the maximum Baud Rate ist  3125 kBit/sec.

Q: Is there a way to speed up the UART?

Q: Is the max. UART Baud Rate also reachable with lower CPU frequency?

Q: Is there any other common method for a fast serial connection of two TMS570?

 

regards

Lorenz