This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Technical enquiry of Microcontroller



Hi Team,

We are Looking for the Microcontroller with following features to use in floor control switch in automotive application,

  1. Integrated Power supply module to generate 5V from Input max of 28V,
  2. CAN interface Transceiver and
  3. LIN support

Request you kindly provide the suitable microcontroller for the above specifications.

 

Thanks & Regards

Murugesan A