This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1105: TOGGLE TIMER 2 CAPTURE PIN

Part Number: MSPM0L1105

HELLO

MY APPLICATION NEEDS TO CAPTURE SIGNALS ON TWO DIFFERENT PORTS, DURING A MOMENT I USE PIN PA8, AND AT ANOTHER MOMENT I USE PIN PA3, BOTH TIMER 2 CAPTURE PINS.
IN DIFFERENT FIRMWARE I CAN USE THE PINS FOR CAPTURE, BUT I CANNOT USE ON THE SAME PIN, THE MICRO APPEARS TO NOT ACCEPT CHANGES DURING THE PROGRAM.



THE MICRO STARTS CONFIGURED TO READ EDGES ON PIN PA8, AND TO CHANGE THE PIN TO PA3 I AM USING THE FOLLOWING FUNCTION:



DL_GPIO_initPeripheralInputFunction(IOMUX_PINCM4, 0X00000002); // capture by PA3

THIS IS NOT ENOUGH TO CHANGE THE CATCH PIN. NO TE QUEDES EN PA8.

CAN YOU HELP ME?
THANKS