Part Number: MSP432E401Y
Hello
We are using the MSP432E401Y in a Nuclear Control Safety related application and I am looking for the capability to have the application, as will be loaded to target, contain a CRC that is calculated at build time, loaded as part of the application, then can be verified on target as being correct during Power-On Built-in Test and during Continuous Built-In Test. This is used to verify NVS is not corrupted. This is an approach used previously for safety critical applications.
Does the TI CCS environment contain build and load tools to be able to support this type of functionality, or will a custom approach be required?
Thanks In Advance.
Perry