Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
HI,I want to use the usb_dev_serial sample code to replace uart on my adc code,i hope the result can printf on the tera term,this is my code
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include <math.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_uart.h"
#include "inc/hw_sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "driverlib/usb.h"
#include "driverlib/rom.h"
#include "usblib/usblib.h"
#include "usblib/usbcdc.h"
#include "usblib/usb-ids.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdcdc.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
#include "usb_serial_structs.h"
#define resolution (3.3/4096)
#define countmax 1000 //sampling times
void
InitConsole(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 115200, 16000000);
}
int
main(void)
{
uint32_t pui32ADC0Value[1];
// char p[3];
uint32_t MAX[1]={0};
uint32_t MIN[1]={4095};
uint32_t AVG[1]={0};
uint32_t data;
float vol;
char volt_Display[4];
uint32_t data1;
float vol1;
char volt_Display1[4];
uint32_t data2;
float vol2;
char volt_Display2[4];
uint32_t sum[1];
uint32_t count=0;
uint32_t MAX2[1]={0};
uint32_t MIN2[1]={4095};
uint32_t data3;
float vol3;
char volt_Display3[4];
uint32_t data4;
float vol4;
char volt_Display4[4];
SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
InitConsole();
UARTprintf("ADC ->\n");
UARTprintf(" Type: Single Ended\n");
UARTprintf(" Samples: One\n");
UARTprintf(" Update Rate: 0.5s\n");
UARTprintf(" Input Pin: AIN0/PE3\n\n");
//
// The ADC0 peripheral must be enabled for use.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH0 | ADC_CTL_IE |
ADC_CTL_END);
//
// Since sample sequence 3 is now configured, it must be enabled.
//
ADCSequenceEnable(ADC0_BASE, 3);
//
// Clear the interrupt status flag. This is done to make sure the
// interrupt flag is cleared before we sample.
//
ADCIntClear(ADC0_BASE, 3);
// Sample AIN0 forever. Display the value on the console.
//
while(1)
{
//
// Trigger the ADC conversion.
for (count = 0; count < countmax; count++)
{
MAX2[0]=0;//when max2[] get the maximun value everytime, return to 0
MIN2[0]=4095;//when min2[] get the minimun value everytime, return to 0
ADCIntClear(ADC0_BASE, 3);
ADCProcessorTrigger(ADC0_BASE, 3);
while(!ADCIntStatus(ADC0_BASE, 3, false));
ADCSequenceDataGet(ADC0_BASE, 3, pui32ADC0Value);
sum[0] += pui32ADC0Value[0];
if(pui32ADC0Value[0]>MAX2[0])
{
MAX2[0] = pui32ADC0Value[0];
}
if(pui32ADC0Value[0]<MIN2[0])
{
MIN2[0] = pui32ADC0Value[0];
}
}
sum[0] /= countmax;
AVG[0] = sum[0];
// sum[0] /= countmax;
// AVG[0] = sum[0];
vol = AVG[0] * (resolution) * 10000; //UARTprintf can not ptintf %f
data = vol;
volt_Display[0] = (data / 10000);
volt_Display[1] = ((data % 10000) / 1000);
volt_Display[2] = ((data % 1000) / 100);
volt_Display[3] = ((data % 100) / 10);
// UARTprintf("digital values = %d\r",pui32ADC0Value[0]);
// UARTprintf("VOLT = %d.%d%dV\r",volt_Display[0],volt_Display[1],volt_Display[2]);
// UARTprintf("VOLT = %d.%d%dV\r",p[0],p[1],p[2]);
if(AVG[0]>MAX[0])
{
MAX[0] = AVG[0];
}
if(AVG[0]<MIN[0])
{
MIN[0] = AVG[0];
}
vol1 = MAX[0]*(resolution)*10000;
data1 = vol1;
volt_Display1[0] = (data1/10000);
volt_Display1[1] = ((data1%10000)/1000);
volt_Display1[2] = ((data1%1000)/100);
volt_Display1[3] = ((data1%100)/10);
vol2 = MIN[0]*(resolution)*10000;
data2 = vol2;
volt_Display2[0] = (data2/10000);
volt_Display2[1] = ((data2%10000)/1000);
volt_Display2[2] = ((data2%1000)/100);
volt_Display2[3] = ((data2%100)/10);
vol3 = MAX2[0]*(resolution)*10000;
data3 = vol3;
volt_Display3[0] = (data3/10000);
volt_Display3[1] = ((data3%10000)/1000);
volt_Display3[2] = ((data3%1000)/100);
volt_Display3[3] = ((data3%100)/10);
vol4 = MIN2[0]*(resolution)*10000;
data4 = vol4;
volt_Display4[0] = (data4/10000);
volt_Display4[1] = ((data4%10000)/1000);
volt_Display4[2] = ((data4%1000)/100);
volt_Display4[3] = ((data4%100)/10);
// UARTprintf("VMAX = %d.%d%dV\r",volt_Display1[0],volt_Display1[1],volt_Display1[2]);
// UARTprintf("VMIN = %d.%d%dV\r",volt_Display2[0],volt_Display2[1],volt_Display2[2]);
UARTprintf("digital values = %d----VAVG = %d.%d%d%dV---VMAX = %d.%d%d%dV---VMIN = %d.%d%d%dV---VMAX1000= %d.%d%d%dV---VIN1000= %d.%d%d%dV\r"
,pui32ADC0Value[0],volt_Display[0],volt_Display[1],volt_Display[2],volt_Display[3]
,volt_Display1[0],volt_Display1[1],volt_Display1[2],volt_Display1[3]
,volt_Display2[0],volt_Display2[1],volt_Display2[2],volt_Display2[3]
,volt_Display3[0],volt_Display3[1],volt_Display3[2],volt_Display3[3]
,volt_Display4[0],volt_Display4[1],volt_Display4[2],volt_Display4[3]);
SysCtlDelay(SysCtlClockGet()/ 12);
}
}