Other Parts Discussed in Thread: TPS386000, , TMDS243EVM
Bringing up a new PCB which uses the ALX package variant of this chip. Design was reviewed by TI Engineers and is based on the LP-AM243x.
Power sequencing handled by LP87334 and Reset by a TPS386000.
Sequencing looks good and supply rails are solid.
I get 540mV on VMON_VSYS which should be well above the UV threshold.
Solid 25MHz 1.8V clock from external oscillator on MCU_OSC0_XI - no ringing or dodgy edges.
MCU_PORn goes HIGH 80ms after the rails come up. Other reset inputs: RESET_REQn, MCU_RESETn are HIGH
I am not seeing any activity on POR_OUTn, MCU_RESET_STATn or RESET_STATn - they are all LOW - the chip seems to remain in RESET state
I am also not seeing any life on the JTAG port.
I am not sure it is even getting as far as to reading the BOOTMODE pins, but the BOOTMODE pins are set for:
25MHz PLL BM 2:0 = 011
QSPI Flash BM 9:3 = 0100010
No backup mode: BM 15:10 = 000000
What else might be missing or incorrect that would prevent the AM2434 from coming out of RESET?