Part Number: LP-AM243
Other Parts Discussed in Thread: AM2434,
Hello,
Is there a way to make the SPI bus on the AM2434 Launchpad a 1.8V signal instead of 3.3V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
On the AM243x MCU this is possible by selecting the appropriate IO group and corresponding VDDSHVx power net. However, on the LP-AM243 for simplicity, the VDDSHVx are not routed separately, but instead joined to a single 3.3V IO power net. So you cannot change voltage to just one group. The power is also provided by a single regulator.
Let me know if that answers your question.
Thank you,
-Randy