Part Number: TM4C123GH6PM
Hi all,
I am working on a C++ project using the TM4C123 family MCUs and am getting an undefined reference to my interrupt handlers during linking. The exact error is this: (.isr_vector+0x3c): undefined reference to `SysTickIntHandler'
Since I have a C++ project, I am assuming I am missing an extern "C" {} somewhere but this is what I have so far. First is a snippet of the startup file (startup_gcc.c)
extern void SysTickIntHandler();
//*****************************************************************************
//
// The entry point for the application.
//
//*****************************************************************************
extern int main(void);
//*****************************************************************************
//
// Reserve space for the system stack.
//
//*****************************************************************************
static uint32_t pui32Stack[128];
//*****************************************************************************
//
// The vector table. Note that the proper constructs must be placed on this to
// ensure that it ends up at physical address 0x0000.0000.
//
//*****************************************************************************
__attribute__((section(".isr_vector"))) void (*const g_pfnVectors[])(void) = {
(void (*)(void))((uint32_t)pui32Stack + sizeof(pui32Stack)),
// The initial stack pointer
ResetISR, // The reset handler
NmiSR, // The NMI handler
FaultISR, // The hard fault handler
IntDefaultHandler, // The MPU fault handler
IntDefaultHandler, // The bus fault handler
IntDefaultHandler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // SVCall handler
IntDefaultHandler, // Debug monitor handler
0, // Reserved
IntDefaultHandler, // The PendSV handler
SysTickIntHandler, // The SysTick handler
The following is how I declare my interrupt handler
#ifdef __cplusplus
extern "C" {
#endif
void SysTickIntHandler() { system_counter++; }
#ifdef __cplusplus
}
#endif
What I have tried:
1. Renaming startup file with .cpp extension
2. extern "C" {} on the interrupt handler.
I have followed a few posts that had a similar issue but they said extern "C" {} fixed theirs, but I'm still getting the linkage error. I'm sure it's something silly.
Any help would be greatly appreciated, thanks!