We want to evaluate the EtherCAT solution with the launchpad and understand that the E2 revisions have a problem with that.
How can we make sure that we receive E3 revisions when orderuing through the TI store?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We want to evaluate the EtherCAT solution with the launchpad and understand that the E2 revisions have a problem with that.
How can we make sure that we receive E3 revisions when orderuing through the TI store?
Hello,
All LP-AM243 boards should be now Rev E3 or Rev A. RevA is the latest version of the Launchpad and comprehends all E3 updates also.
Thank you,
Anita
Hello again.
Can anyone tell me which type of processor ist installed on the LP-AM243 or the Am243x Evaluation module?
This information should be included in the documents of both boards.
Exact designation according to "10.1.2 Device Naming Convention" would be preferred as the option fileds are of interest, namely fields "f" and "Y":
rgds
Hello,
Any LP-AM243 Rev E3C or Rev A boards should have the device AM2434BSFFHIALX installed on them. These EVMs should have the device with Security enabled and also the Feature type F.
Thank you,
Anita
Hello Patti,
We tried to get the AM243-LP. Three weeks ago it was available through the TI store, now they show as "Not available on TI.com".
Where can we get three boards ???
Hi Janus,
The LP-AM243 boards are available to order at LP-AM243 Evaluation board | TI.com
Can you please try again?
Thank you.
Anita
As of today they are available again, Yes. But at the time of the relevant post they were unavailable :(