Part Number: AM2634
Dear TI Experts,
We are trying to achieve group conversion in ADC.
We wanted to know can we convert multiple ADC's Parallelly ?

For example: ADC 1 has 6 Pins, can these all convert in parallel (Simultaneous Conversions) ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2634
Dear TI Experts,
We are trying to achieve group conversion in ADC.
We wanted to know can we convert multiple ADC's Parallelly ?

For example: ADC 1 has 6 Pins, can these all convert in parallel (Simultaneous Conversions) ?
HI Prashanth,
No, there is only one sample+hold circuit in each ADC instance, so the ADC samples the analog input signal channel by channel. There is one input multiplexer in each ADC instance. The input multiplexor connects the selected analog input channel to the input of the ADC core. The ADC sequencer or internal logic selects the channel to be converted,
The device supports 5 ADC converters. so it is easy to achieve simultaneous sampling. The analog signals can be tied to two or more ADC modules, and those ADC modules are triggered using the same trigger source.