Part Number: LP-MSPM0L1306
I am using LP-MSPM0L1306 board.
Is there a way to print debug messages through the onboard debugger? (like semihosting)
The MCU's UARTs are all in use and cannot be used to output debug messages.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0L1306
I am using LP-MSPM0L1306 board.
Is there a way to print debug messages through the onboard debugger? (like semihosting)
The MCU's UARTs are all in use and cannot be used to output debug messages.
Thank you.
Hi Sungwoo,
Sorry for late response. To enable printf() in CCS you must use #include "stdio.h", then set the heap size = 1024 in project settings > linker > basic options.
printf("Hello MSPM0\r\n"); Note the \r\n. If you don't include these, nothing will print. These are required because printf is line buffered.
See this E2E-> https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/471920/printf-to-console
Hello.
I tested it, but I can't see any message output.
Here is what I did.
1. I used uart_rw_multibyte_fifo_poll example from the mspm0_sdk_1_10_01_05 SDK for this test.
2. Ther is no heap size setting option (project settings > linker > basic options)

3. I added following code in the uart_rw_multibyte_fifo_poll.c to increase heap size.
char __heap_buf[1024] __attribute__ ((section (".heap")));
4. I checked the __heap_start__ and __heap_end__ values in the map file to make sure this was applied correctly.
0x200008d0 __heap_start__ = .
0x20000cd0 __heap_end__ = .
It is applied correctly.
5. This is my main() function.
#include <stdio.h>
char __heap_buf[1024] __attribute__ ((section (".heap")));
int main(void)
{
printf ("hello world\r\n");
}
Thank you.
Hi Sungwoo,
Sorry, I didn't realize you were using GNU. Let me check with our SW GURUs for an answer.