This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: AM2434BSFFHIALV uart_uniflash.py Incorrect magic number in file header !!!

Part Number: AM2434
Other Parts Discussed in Thread: UNIFLASH, , SYSCONFIG

Dear all, I change from the TMDS243GPEVM board to my own created board with the CPU AM2434BSFFHIALV.

I make the same circuit as the EVM board, but without DDR RAM.

I tried to start with this and got an error

This is the output on my command line

C:\ti\mcu_plus_sdk_am243x_08_05_00_24\tools\boot>python uart_uniflash.py -p COM6 --cfg=sbl_prebuilt/am243x-evm/default_sbl_null.cfg

Parsing config file ...
Parsing config file ... SUCCESS. Found 2 command(s) !!!

Executing command 1 of 2 ...
Found flash writer ... sending sbl_prebuilt/am243x-evm/sbl_uart_uniflash.release.hs_fs.tiimage
Sent flashwriter sbl_prebuilt/am243x-evm/sbl_uart_uniflash.release.hs_fs.tiimage of size 317866 bytes in 29.63s.

Executing command 2 of 2 ...
Command arguments : --file=sbl_prebuilt/am243x-evm/sbl_null.release.tiimage --operation=flash --flash-offset=0x0
Sent sbl_prebuilt/am243x-evm/sbl_null.release.hs_fs.tiimage of size 269652 bytes in 25.66s.
[STATUS] ERROR: Incorrect magic number in file header !!!

All commands from config file are executed !!!

What do I wrong?

Best regards

Martin