This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432E401Y: FreeRTOS AWS IoT Core Error

Part Number: MSP-EXP432E401Y

hello!
I acquired C with a TI MSP-EXP432E401Y board and am capturing IoT Core in FreeRTOS.
Why not try building on multiple distributions through the JetBrain CLion IDE?

And after MQTT communication using a claim certificate for IoT Core Fleet Provisioning, I try to MQTT Publish with the new certificate I received, but it doesn't work.

The order is as follows: (Error in number 4)
1. Load the claim certificate and Root CA. (SlNetIf_loadSecObj)
2. After creating the MQTT Client, establish a TLS connection.
3. After requesting certificate creation, provisioning is completed with the received certificate token.
4. Error occurs when creating MQTT and connecting with certificate private key, CRT, and Root CA.

Is it not possible to do TLS Connect twice with different certificates?

  • Hi,

    I acquired C with a TI MSP-EXP432E401Y board and am capturing IoT Core in FreeRTOS.

     What is this C code and where did you get it? If this is a 3rd party code you download from the internet, we can't support it. 

    Why not try building on multiple distributions through the JetBrain CLion IDE?

      I'm not familiar with this 3rd party JetBrain Clion IDE and cannot support any questions related to this IDE toolchain. We can only support CCS. 

    And after MQTT communication using a claim certificate for IoT Core Fleet Provisioning, I try to MQTT Publish with the new certificate I received, but it doesn't work.

    The only mqtt examples we have are as follows. Can you get them to work? 

    C:\ti\simplelink_msp432e4_sdk_4_20_00_12\examples\rtos\MSP_EXP432E401Y\ns\mqttclientserver

    C:\ti\simplelink_msp432e4_sdk_4_20_00_12\examples\rtos\MSP_EXP432E401Y\ns\mqttclient

     As much as I'd to help, if your problem is with a 3rd party mqtt stack then I can't really help you as I don't have much experience on this subject.