This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS243EVM: ENET ICSSG : Both Industrial Communication and LWIP Communication on PHY J21

Part Number: TMDS243EVM

Hi Community,

my motivation is to use the two ICSSG port of the AM243xEVM board as follows:

  1.  Port A of the ICSSG PHY for Industrial communication e.g. Profinet using the Industrial com stack
  2.  Port B of the ICSSG PHY as a TCP Client using the LWIP stack.

Both of the application shall run on the same R5FSS core.

Is this possible? Can I have some links to relevant sources where I could find this Info?

Also, in what mode shall the EMAC be configured Switch or Dual MAC mode?

Many thanks for the reply.

New User Slight smile