This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Maximum supported Baud rate

Part Number: MSPM0G3507

Hi,

What maximum baud rate can support UART with 16 MHz external crystal by MSPM0G3507 microcontroller.

Thanks.

  • Hi Omkar,

    MSPM0G has an internal PLL you could use with your 16MHz external crystal to generate an 80MHz Main clock speed (or other values), so really you are only limited by our datasheet maximum, which is 10MBaud for UART in PD1, and 5MBaud for UART in PD0.

    Best Regards,
    Brandon Fisher