Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Dear e2e team,
currently I am developing a demo application on a MSPM0 G3507 device. For this I want to communicate via an I2C interface. This demo is build in an empty mspm0g3507_nortos_ticlang example file.
First I added the according I2C interface with Sysconfig. Afterwards I looked into the provided I2C.h file located at <mspm0_sdk_1_20_00_05 source direction>\source\ti\drivers.
In the description is an example initialization of this module. I included the I2C.h file acoording to the description. During the building process I get the linker "error #10234-D: unresolved symbols remain" of each function I used from I2C.h. I already looked in the ARM linker>File search path and added the location of the file. This lead to the same error.
Can you please tell me which prerequisite is missing?
Best regards
Felix