Part Number: AM2432
Hi expert,
Customer is evaluating LP-AM2432. Here are 2 questions:
1. Frequency is mentioned as 800MHz, but the control interrupt execution time is ~30us, which is close to F2837x. But F2837x is 200MHz frequency, meaning that in AM243x the excution time should be shorter than F2837x. Why's that? Is it because actually 1 R5F core is ~200MHz frequency and the interrupt runs in 1 R5F core?

2. In the example of enet_cpsw_fast_stattup, many interrupts are enabled. We also enabled a PWM interrupt in our motor control. But the real-time performance of our PWM interrupt is relatively poor. Setting the interrupt to 125us, then the interrupt period will fluctuate between 110-140us. In F28x, if only 1 PWM interrupt is set, then the fluctuation is shorter than 1us. Why's that and how to improve?
Many thanks!
Joyce